Skip to content

Link to ArrowNAC.com Primary and Secondary Navigation

Manufacturers

Infinite Power Solutions

Infinite Power Solutions, Inc. (IPS)—a U.S. clean-technology company—is a global leader in manufacturing solid-state, rechargeable, thin-film micro-energy storage devices for embedded applications. Founded in 2001, IPS is privately held with corporate headquarters and volume manufacturing in Littleton, Colo. The company is the only ISO 9001 certified manufacturer of solid-state, thin-film batteries. THINERGY® Micro-Energy Cell (MEC) products provide unprecedented efficiency in micro-energy storage and uniquely enable ambient energy-harvesting solutions to create miniature, autonomous, perpetual power supply solutions.

 

 

About Infinite Power Solutions

Infinite Power Solutions, Inc. (IPS)—a U.S. clean-technology company—is a global leader in manufacturing solid-state, rechargeable, thin-film micro-energy storage devices for embedded applications. Founded in 2001, IPS is privately held with corporate headquarters and volume manufacturing in Littleton, Colo. The company is the only ISO 9001 certified manufacturer of solid-state, thin-film batteries. THINERGY® Micro-Energy Cell (MEC) products provide unprecedented efficiency in micro-energy storage and uniquely enable ambient energy-harvesting solutions to create miniature, autonomous, perpetual power supply solutions.

Product Highlights

Infinite Power Solutions, Inc. (IPS) offers a line of award-winning THINERGY® Micro-Energy Cells (MECs), a type of rechargeable solid-state battery (SSB), as an innovative new technology that provides a capable and cost-effective alternative to lithium, alkaline, thin-film and other traditional batteries, as well as supercapacitors. THINERGY MECs are the highest performing and most powerful batteries for their size.

THINERGY® MICRO-ENERGY CELLS (MECs)

IPS’ innovative THINERGY® Micro-Energy Cells (MECs) are revolutionary solid-state, rechargeable, energy storage solutions that serve a variety of vertical markets. These paper-thin MECs are flexible and provide unrivaled cycle life and power performance. Able to operate in temperatures ranging from -40ºC to +85ºC, these ultra-thin MECs offer extremely low self discharge rates, low cell resistance and high power—making THINERGY the industry leading micro-energy storage offering. THINERGY Micro-Energy Cells are ideally suited for use with all forms of ambient energy harvesting techniques for recharging—such as solar, thermal, RF, magnetic and vibration energy—delivering a safe, reusable and clean power source for today’s electronic devices and systems.

IPS-EVAL-EH-01: ENERGY HARVESTING EVALUATION KIT

This universal energy harvesting kit is ideal for developing and evaluating various energy harvesting solutions for self-powered applications. This kit incorporates a THINERGY® MEC201-7S (0.7 mAh capacity) device, the Maxim MAX17710 Energy Harvesting Power Management IC (PMIC) and an amorphous silicon solar panel from Sanyo/Amorton. This kit will also connect to any external (user provided) AC & DC charge sources up to 5V & 150mW. An integrated boost converter enables low voltage energy sources >200mV as charge sources.

ADP-101: THINERGY Application Development Platform

The ADP is a unique and comprehensive evaluation and application development tool used to demonstrate the many performance advantages of THINERGY Micro-Energy Cell (MEC) products. The ADP-101 greatly simplifies the typical lab setup for micro-battery testing and is very useful for evaluating battery performance, effectiveness of charging circuits using ambient energy harvesting, and overall system development of the user’s end application. In addition, the ADP provides data logging over a USB port, allowing the user to capture and record test data, including discharge, recharge, energy harvesting, and application emulation data. Kit includes: 3 MEC101 devices mounted on a PCB that plug into the ADP for evaluation purposes.

ADP-201: THINERGY Application Development Platform

The ADP is a unique and comprehensive evaluation and application development tool used to demonstrate the many performance advantages of THINERGY Micro-Energy Cell (MEC) products. The ADP-201 greatly simplifies the typical lab setup for micro-battery testing and is very useful for evaluating battery performance, effectiveness of charging circuits using ambient energy harvesting, and overall system development of the user’s end application. In addition, the ADP provides data logging over a USB port, allowing the user to capture and record test data, including discharge, recharge, energy harvesting, and application emulation data. Kit includes: 3 MEC201 devices mounted on a PCB that plug into the ADP for evaluation purposes.

Offers

To view a list of special offers please follow the link below.

View All >>

Back To Sub-Section Navigation

Events and Training

One moment...

While we retrieve events and training.

loading


View All >>

Back To Sub-Section Navigation

Link to ArrowNAC.com Tertiary Navigation