Link to ArrowNAC.com Primary and Secondary Navigation
Contact an Arrow Service Representative • 1-877-237-8621
Established in 1944, Murata Electronics has focused on the R&D of functional ceramic materials and the development of their potential applications. Ceramic technology is growing increasingly important as a key driving force in the creation of a new electronics revolution for the 21st century. Murata's commitment to this endeavor has resulted in their introducing a wide, diverse range of innovative Ceramic Electronic Components while becoming one of the world's largest passive component manufacturers in the process . Murata Electronics N.A., Inc.'s product line includes Capacitors, Coils (inductors), EMI suppression filters, ESD Devices, Piezo Alarms , Piezo Buzzers, Piezo Speakers, Ceramic Crystals, Ceramic Resonators, RF Connectors , RF Filters , RF Modules , Sensors and Thermistors.
About MurataEstablished in 1944, Murata Electronics has focused on the R&D of functional ceramic materials and the development of their potential applications. Ceramic technology is growing increasingly important as a key driving force in the creation of a new electronics revolution for the 21st century. Murata's commitment to this endeavor has resulted in their introducing a wide, diverse range of innovative Ceramic Electronic Components while becoming one of the world's largest passive component manufacturers in the process. Murata Product HighlightsMurata Electronics , the leader in ceramic based material technology for electronic components and modules. GR Series GR series Ceramic (MLCC) Capacitors available from 1pF to 100uF and EIA sizes from 01005 to 1206 case sizes. Used to support various consumer, industrial and automotive applications. ECAS Series ECAS series Polymer Aluminum Electrolytic Capacitors available from 10uF to 470uF and EIA 7343 case sizes. Used to support various consumer, industrial and commercial applications where low ESR and high capacitance is required. BLM Series BLM series Chip Ferrite Beads available in EIA 01005 to 0805 case sizes and current ratings up to 6A. Used to suppress EMI / RFI noise in consumer, industrial and automotive applications. Ceralock Ceramic Resonators Ceralock Ceramic Resonators in surface mount packages available from 2 MHz to 70 MHz. Ideal as a low cost clock source to support industrial, consumer and automotive micro controller based applications. |
L Series Chips LQP, LQW, LQH, and LQM series chip inductors offered in EIA 01005 to 2525 case sizes. Available in wire wound, multi layer and film type Murata offers a wide range of chip inductors for power, general and RF applications. P Series Chips PKB, PKL, and PKM series Piezo Electric Alarms & Buzzers available in surface mount and leaded styles. Using Murata's processing technology and unique piezoelectric material we offer Piezo speakers, Piezo diaphragms, Piezo buzzers, Piezo sounders and Piezo ringers for a range of consumer, industrial and automotive applications. LXES Series LXES series ceramic and silicon ESD protection devices in surface mount packages supporting from 1 to 6 channels. Ideal to protect high speed circuits through I/O ports from electrostatic discharge in consumer and industrial applications. Thermistors NCP, NTP, PRF, PRG, and PTG leaded and surface mount NTC/PTC Thermistors. Ideal for overheat and over current protection for virtually all consumer, commercial, industrial and automotive applications. |
Capacitors (35492)
Circuit Protection (938)
Frequency Controls (507)
Magnetics (1949)
Magnetics - Inductors (2274)
Resistors (5975)
PEMCO (496)
Audio (89)
Power Supplies (215)
Clocks & Timers (8)
Communication (2)
Linear (2)
Power (13)
RF/MW (176)
Sensors (48)
One moment...
While we retrieve events and training.